7/18/2021 8:05 PM | |
Joined: 1/4/2018 Last visit: 7/17/2023 Posts: 9 Rating: (0) |
Is there version for TIA Portal V17 anywhere? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/19/2021 05:56:02New subject after splitting |
|
7/18/2021 8:52 PM | |
Joined: 3/30/2020 Last visit: 5/16/2024 Posts: 4508 Rating: (943) |
Updater that comes with TIA Portal V17 is shipped with TIA Portal. The updater software will only offer software version that you already have installed. The updater software cannot offer V17 if you have not installed it. Download the trial version here: Or do you have another reason for your query? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
7/20/2021 10:23 AM | |
Joined: 9/10/2012 Last visit: 5/10/2024 Posts: 67 Rating: (5) |
I agree. For me, main issues are: - all update buttons at start are disabled and turn on after a random time, sometimes seconds, sometimes half an hour, sometimes never; there is nothing that tells me what's going on - if I try to donwload or install something the progress bar stand still for an endless time. After a week of usage I'm still waiting for the first successful update. - from time to time, I receive Windows notifications about available updates, if I click them a new version of TIA Admin opens, so everything restart from the beginning - I had a lot of installation problems, a certificate was missing and I had to solve it by myself (this post: certificate issue) Maybe it's my fault because I'm used to Firefox and I don't want to change it, maybe using Chrome is better, I don't know. |
Follow us on