4/29/2024 8:42 PM | |
Joined: 1/16/2012 Last visit: 6/6/2024 Posts: 9 Rating: (0) |
Thx, Second thought: copy the complete folder from a working PC to the defective PC: folder "C:\Windows\SysWOW64\config\systemprofile\AppData\Local\Microsoft\Microsoft SQL Server Local DB\Instances\MSSQLLocalDB" Now it works. I've copied the entire directory to several ZIP files. (File size max 5 MB was max to upload, so 4 files were made. MSSQLLocalDB.zip, MSSQLLocalDB.z01, MSSQLLocalDB.z02, MSSQLLocalDB.z03 The .z0? was not an allowed extension to upload to Siemens so I changed its name. (I use ? in stead of 1/2/3...) Retrieve them all, rename MSSQLLocalDB_z0?.zip to MSSQLLocalDB.z0? AttachmentMSSQLLocalDB.zip (3 Downloads) |
4/29/2024 8:43 PM | |
Joined: 1/16/2012 Last visit: 6/6/2024 Posts: 9 Rating: (0) |
File 2/4
AttachmentMSSQLLocalDB_z01.zip (4 Downloads) |
4/29/2024 8:43 PM | |
Joined: 1/16/2012 Last visit: 6/6/2024 Posts: 9 Rating: (0) |
File 3/4
AttachmentMSSQLLocalDB_z02.zip (4 Downloads) |
4/29/2024 8:45 PM | |
Joined: 1/16/2012 Last visit: 6/6/2024 Posts: 9 Rating: (0) |
File 4/4. AttachmentMSSQLLocalDB_z03.zip (5 Downloads) |
Follow us on