4/4/2024 9:20 AM | |
Joined: 7/9/2015 Last visit: 5/29/2024 Posts: 3850 Rating: (564)
|
Hi, You can use the open communication by means of the TSEND_C and TRCV_C instructions for data exchange over the integrated PROFINET interface of the S7-1200. Please check this Link to an application example: https://support.industry.siemens.com/cs/ww/en/view/67196808 Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
4/4/2024 2:24 PM | |
Joined: 3/30/2020 Last visit: 6/6/2024 Posts: 4573 Rating: (950) |
The port on the PLC is an Ethernet port certified for the Profinet protocol. This detail has no influence on your project. The PLC Ethernet port puts out the Ethernet TCP which you require. You can use raw 'sockets' in Python if you wish to do so. Have a look at an older forum topic: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on