7/24/2023 3:32 PM | |
Joined: 1/4/2007 Last visit: 5/31/2024 Posts: 1128 Rating: (174)
|
Hello Valter_pv, 1. The s_IO_DATA.ERROR_CODE goes only to TRUE, when there is a data- or command-error. 2. The operating errors, technology errors and command errors in DR32 (Format: Word) are in reality single bit error-messages. Attached you can see the meaning of the single bits. 3. I will check the meaning of the „DR32.ERR_CODE_S7_INTERFACE“. 4. The difference between the FB WP321DR version 3.1 and 4.8 is: - the firmware of the PLC is less than V2.0: You have to use the FB WP321DR version 3.1 - the firmware of the PLC is equal to or higher than V2.0: You have to use the FB WP321DR version 4.8. Best regards Siwarexi
Attachmentbit messages.zip (399 Downloads) |
This contribution was helpful to1 thankful Users |
7/28/2023 7:04 AM | |
Joined: 10/18/2017 Last visit: 5/31/2024 Posts: 23 Rating: (0) |
thank you Siwarexi |
Follow us on