12/15/2009 6:34 PM | |
Joined: 2/10/2006 Last visit: 3/21/2024 Posts: 147 Rating: (12) |
You can try with PLC Workshop for Siemens 505. This is a Windows package that is fully compatible with Tisoft programs. You can download a trial version from http://www.fast-soft.com/download.php?view.295 At least you'll be able to make sure that your hardware connection is working ok. |
12/15/2009 7:01 PM | |
Posts: 510 Rating: (117)
|
Here is the link to the last TISOFT manual which covers version 6.3 to 7.1. http://support.automation.siemens.com/US/view/en/17518681 Sections 1.4 and 1.5discuss installingTISOFTin Windows (95) and starting TISOFT from a shortcut on the desktop or the command line. I have TISOFT 7.1 running on Windows XP SP2 and SP3 communicationg using the Serial Port, COM,1 on DELL M70 and 4300 laptops. I normally start it with the Desktop shortcut. I checked the properties for the shortcut and I did not do anything special to accomplish this. |
Follow us on