5/14/2024 6:42 PM | |
Joined: 3/3/2010 Last visit: 6/7/2024 Posts: 8 Rating: (0) |
Hi to all I'm traying to transfer an Audit Trail license (Wincc Unified Audit Basis V18.0) to the Unified Comfort Panel (MTP700) using the Automation License Manager but is not working. Everytime that I try to start the connection with the panel, the ALM shows me this error: "transfer error: 16842752 (0x1010000) - Connection error". I have always used this same license transfer method with the old Comfort Panels and I have never had any problems. On the other hand, it is important to note that with TIA PORTAL V18 I have been able to download programs to my Unified Panel without any problems. I also have a correct connection with ProSave to extract backups. Is there a different procedure for transferring licenses to Unified Comfort Panels? AttachmentEvidence.zip (20 Downloads) |
Follow us on