3/8/2024 6:54 AM | |
Joined: 3/11/2019 Last visit: 6/11/2024 Posts: 1461 Rating: (264) |
Hi Roby, yes, in this case, the error is caused due to the difference for the CP. Because it is not allowed to confiure a newer firmware in hw config, as the device itself has. You can either try to change the firmware in hwconfig -> change device, choose firmware V2.xx in drop down menu and place this one in hw config. Or you can try a firmware update of the CP itself. Delivery release of firmware update V3.0.37 for CP 1543-1.regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on