11/30/2011 8:56 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Dear Sandman As per the Siemens Manual the Modbus communication has been tested only with RS232 port and certain Modicon PLCs Models only.It also says that it has neither been tested nor recommended with other ports / PLCs. I am trying the same with a TP 177B ( Configured with WInCC Flexible 2008 SP2 ) I do not get any errors during configuration / downloading. I have tried using RS485 as well as RS422 ( I have also changed DIP switches asshown on back of TP ).. However there is no Transmit/Receive happening from the TP177B ( Configured as Modbus Master ). TP is working normally when I check it with MPI / Profibus. It seems that Modbus Driver is not designed to work with RS485 / RS422 ports. If there is a driver update which supports RS485 / RS232 also, I would like to know. Thanks Navnag |
Last edited by: O_Moderator at: 11/30/2011 10:17 AMnew subject after splitting from /tf/WW/en/Posts/63250#top There is no such thing as the last bug in a program |
|
11/30/2011 10:18 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Modbus Communication with TP177B Best regards O_Moderator |
Follow us on