5/15/2024 7:29 AM | |
Joined: 6/10/2022 Last visit: 5/15/2024 Posts: 2 Rating: (0) |
Hello everyone, I found this discussion that I think could help me a lot. I have recently bought an ATLAS MK5 gateway that I need to interface a Leybold Coolpak5000 compressor with a Siemens S7-1500 PLC. The compressor has a CAN interface and I would like to use the gateway to convert the CAN into profibus and connect the PLC. I was able to establish the communication between the compressor and the gateway but the plc is not able to see the gateway: the node is "not accessible" as it appears in the Siemens software. Please, can you send me the right procedure to follow in order to configure the communication between the gateway and the PLC through the profibus connection? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/15/2024 08:44:54New subject after splitting |
|
5/15/2024 8:47 AM | |
Joined: 6/19/2017 Last visit: 5/31/2024 Posts: 8110 Rating: (165) |
Closed cause question posted twice. The second thread with the subject Connect ATLAS COPCO gateway MK5 to Siemens S7-1500 via PROFIBUS is published within the conference Communication / Networks. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on