11/8/2023 11:45 AM | |
Joined: 3/6/2020 Last visit: 6/2/2024 Posts: 34 Rating: (0) |
Hello, how to write/make (in LAD) a condition so that a mathematical operation is performed conditionally ? |
11/8/2023 1:33 PM | |
Joined: 3/11/2019 Last visit: 6/12/2024 Posts: 1464 Rating: (264) |
Maybe via jump. conditional jump to the arithmetic operation or unconditional jump over the operation. S5-90U/S5-95U Programmable Controller System Manualregards sancruz |
Last edited by: sancruz at: 11/08/2023 13:38:52Feedback appreciated, please rate |
|
11/8/2023 2:05 PM | |
Joined: 3/6/2020 Last visit: 6/2/2024 Posts: 34 Rating: (0) |
I can't use JUMP in LAD. It is not basic instraction. |
11/18/2023 3:51 PM | |
Joined: 5/6/2010 Last visit: 6/2/2024 Posts: 1966 Rating: (274) |
Hello, yes, you need a FB to use the function JMP.. Maybe is this manual helpful for you (chapter 7) or this training manual regards Attachment6ES5_998-0MA24.pdf (520 Downloads) |
Last edited by: CaOd at: 11/18/2023 15:54:58Last edited by: Jen_Moderator at: 11/20/2023 12:14:33PDF added from link. |
|
12/12/2023 6:57 PM | |
Joined: 3/6/2020 Last visit: 6/2/2024 Posts: 34 Rating: (0) |
CaOdCould you send some photo from Step5, where is jump instruction (Jump to label) ? |
12/26/2023 6:59 PM | |
Joined: 5/6/2010 Last visit: 6/2/2024 Posts: 1966 Rating: (274) |
Hello plcspace, I have a look at a few "old" documentations. If I read it correct you must move the cursor under the output and then you should press "Shift F4". Then you can select the jump then you can write the label name over the output. I hope this is a little bit more helpful. There aa link to a document in German language: https://www.sps-lehrgang.de/sprungfunktionen-in-kop/ At the follow link you can find some information's about Step5 regards |
12/29/2023 12:47 PM | |
Joined: 12/29/2023 Last visit: 12/29/2023 Posts: 3 Rating: (0) |
your welcome |
1/12/2024 8:27 AM | |
Joined: 3/6/2020 Last visit: 6/2/2024 Posts: 34 Rating: (0) |
Hello CaOd, Could you upload this a few "old" documentations ? |
3/18/2024 4:24 AM | |
Joined: 3/6/2020 Last visit: 6/2/2024 Posts: 34 Rating: (0) |
Hello CaOd, Yes, i would like "translate" this code from STL to LAD. Could you make some photo "how do it" step by step ? |
Follow us on