12/6/2005 4:40 PM | |
Posts: 9 Rating: (0) |
I have Step7 5.3. I've download servicepack sp1 sp2 sp3. Can I install only sp3??? |
12/6/2005 4:55 PM | |
Joined: 8/25/2005 Last visit: 5/15/2024 Posts: 1161 Rating: (110) |
Hello bzykus, in the following document it is written, are the prerequisites for the installation discriped. If I understand right, SP3 can be installed, if you have only STEP7 V5.3 without any servicepack. Service Pack 3 for STEP 7 V5.3 and STEP 7 Professional Edition 2004 Best regards Sabine |
12/6/2005 5:19 PM | |
Posts: 9 Rating: (0) |
I've already installed SP3 to Step7 5.3. I wonder if sp3 contain all upgrades from sp1 and sp2. So there is no need to install sp1 sp2 and in the end sp3? |
12/7/2005 2:13 AM | |
Posts: 52 Rating: (8) |
The sp1 sp2 is not necessaries if you have sp3. |
Follow us on