4/24/2024 12:44 PM | |
Joined: 5/6/2022 Last visit: 6/6/2024 Posts: 420 Rating: (83) |
Hi AutoGen_7661683, In this case I would also recommend performing a reset of the panel to factory settings: "How do you do a SIMATIC HMI operating system update (firmware update, OS update) on operator panels or perform a "Reset to factory settings"?" I would also check that you have the latest update of the TIA Portal version installed, that you comply with the limitations of the panel ("SIMATIC HMI HMI devices Comfort Panels: Scope of functions with WinCC") and see if the same thing happens to you with a new project. Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on