4/24/2024 11:55 AM | |
Joined: 10/31/2023 Last visit: 5/21/2024 Posts: 13 Rating: (0) |
I'm trying to change some parameters like 2000/4-5 >1, 39080 >2048, 3680 >1, these just because the axis still doesn't locate in the exact position and fires, do you know any way to remove this linear scale from the x axis?
AttachmentPictures.zip (26 Downloads) |
Last edited by: Jen_Moderator at: 04/25/2024 06:48:06All pictures added as .zip file. |
|
4/29/2024 1:29 PM | |
Joined: 10/31/2023 Last visit: 5/21/2024 Posts: 13 Rating: (0) |
THANK YOU IN ADVANCE FOR THE FEEDBACK, I HAVE RETURNED THE REQUIRED BACKUP, EVERYTHING IS OK, IT DOESN'T OCCUR BUT THE 20190 FAILURE, BUT I STILL HAVE TO REMOVE THE LINEAR SCALE ON THE X AXIS, I AM SENDING YOU PHOTOS OF THE MACHINE DATA FOR YOU TO CHECK
AttachmentImages.zip (12 Downloads) |
Last edited by: Jen_Moderator at: 04/30/2024 07:45:20All images added as .zip file. |
|
4/30/2024 2:13 AM | |
Joined: 10/17/2007 Last visit: 5/30/2024 Posts: 3992 Rating: (345)
|
I do not need so many pictures, 1 st and 2nd should be in one page--one picture. I think you only need change 2000/4-5 to 1 also you need try to help yourself--I think you spindle is the 1st axis , then X is 2nd. and Y may be 3rd. I see Y axis has only one encoder --motor encoder --post Y axis NC MD--one page only ending at 2001/4-5 --I think they should be FDD 3.0 and FDD 3.1
AttachmentAXIS_config_Basic--add.pdf (14 Downloads) |
If you like my comments please |
|
4/30/2024 2:23 AM | |
Joined: 10/17/2007 Last visit: 5/30/2024 Posts: 3992 Rating: (345)
|
I attach your picture--in zip, please try to make these 2 in one picture and make the same picture of Y Axis POST here Attachment840C-611D-X-AX-1.zip (13 Downloads) |
If you like my comments please |
|
Follow us on