2/28/2024 10:33 AM | |
Joined: 2/8/2019 Last visit: 4/3/2024 Posts: 2 Rating: (0) |
Hi, can any expert please clarify this product 6AG4104-5JH35-2AD1 Specially in the 5JH35 part. The 3 in the "5JH35" part in Tia Selection Tool mean: Housing with drive cage type A (for frontside mounted removable tray), blue chromated but in 2023 product catalogue which can be downloaded in this link Catalogue page 410 said that: Enclosure with drive cage type B (for internal installation/ 0.2 g vibration, 2 g shock); coated Which one is the correct description? |