4/25/2024 12:48 PM | |
Joined: 9/7/2023 Last visit: 5/22/2024 Posts: 24 Rating: (0) |
Hello everyone. Thanks for your help. I have a similar issue. SFC51-"RDSYSST" works great for me on this CPU: CPU 317-2 PN/DP - Profinet in X2 of the CPU Firmware V3.2.12 6ES7317-2EK14-0AB0 SZL_ID: 694; INDEX: 64 (100 in decimal) But all the same settings won't work on the following CPU: CPU 319-3 PN/DP - Profinet in X3 of the CPU Firmware V2.4.0 6ES7 318-3EL00-0AB0 I've tried SZL_ID: 694 and 294, and neither work. (the busy signal never seems to come on). Is SFC51 compatible with this CPU + Firmware. I know FB126 is not compatible, as the firmware is too old. Is there a different diagnostic tool that will work instead? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/26/2024 05:37:35New subject after splitting Last edited by: Jen_Moderator at: 04/29/2024 11:15:35Headline optimized. |
|
5/3/2024 12:41 PM | |
Joined: 9/7/2023 Last visit: 5/22/2024 Posts: 24 Rating: (0) |
Giving this a bump, wondering if anyone knows about this. |
Follow us on