4/24/2024 8:35 AM | |
Joined: 3/11/2019 Last visit: 5/21/2024 Posts: 1425 Rating: (257) |
Hi, as already mentioned, this can happen if old/wrong data are stored on the MMC. Important: Do not format/delete a MMC via windows and standard cardreader! In STEP 7 (TIA Portal), how do you format an MMC or MC and why does a message appear saying that the SDB 7 is not loaded?Which devices can you use to read from, write to or delete from an S7-300 MMC (Micro Memory Card) outside the CPU?How do you delete the data on an MMC (micro memory card)?regards sancruz |
Feedback appreciated, please rate |
|
Follow us on