4/17/2024 9:49 AM | |
Joined: 3/19/2019 Last visit: 6/6/2024 Posts: 23 Rating: (0) |
Dear Experts, Please help me slove my issue. Problem details. PLC was running ok without any error, suddenly today morning NODE - 5 ( SEW communication module for sew drive communication) fault occurred, after fault reset NODE fault reset and when i give command to sew drive it start and run for 10sec again node 5 fault was coming, in that SEW module total 7drives connected, out of 7 drives 5 was working ok after fault reset. When i give the command to 6 and 7 it just starts for few sec and again node fault was comming if i reset error goes and again comes during next start. I cheanged the SEW communication module also but still the problem is not resloved. I changed the profibus connecter and cable too. Please hlep me reslove this issue. Thanks VMK AttachmentDiagnose.txt (22 Downloads) |
Follow us on