4/30/2024 1:07 PM | |
Joined: 3/30/2020 Last visit: 5/21/2024 Posts: 4520 Rating: (943) |
There is a way to combine multiple TIA Projects with each other and retain the ease of use that you would have had if all were in one project. You do not need to resort to absolute addressing. What you do need is to configure a "device proxy". It is a stand-in (ghost) of the device within the alternate project. This technique can also be followed to combine Step7 classic with WinCC (TIA Portal). In your case the Wincc (TIA Portal) project will have a stand-in proxy device that represents the data structures of the 2nd PLC. Have a look at the following information: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on