12/20/2016 4:21 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (307) |
Hello, I undertstand that your major concern is not to make changes in the router where the PLC is located. See application examples. Installation and Management of Secure Remote Networks with SINEMA Remote Connect (Video) |
Best regards |
|
This contribution was helpful to1 thankful Users |
12/21/2016 9:26 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
As mentioned above VPN is way better to connect to any device. https://www.shodan.io/ is a search engine which can be used to find any open connection and even more. So security would be a great deal. If you want to set up VPN you can choose between software, hardware or hard and software solution. On my side the customer uses a combination of hardware VPN Server with hardware VPN Client. This makes it a IT issue to set up the connection between the Server and Client part and the rest is just transparent for the users. Full access as if you where in the same network. Siemens has scalance with this features, too. |
~(‾▿‾)~ |
|
12/21/2016 11:08 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (307) |
Hello, And if the router has a variable public IP address, you must use a public name that must be registered in the Internet. Otherwise is more difficult to know to which IP address the tunnel must connect. The tunnel will connect to a name instead of an IP address. |
Best regards |
|
This contribution was helpful to1 thankful Users |
5/14/2024 12:24 PM | |
Joined: 6/19/2017 Last visit: 5/29/2024 Posts: 8119 Rating: (165) |
New question published by EngSamer is split to a separate thread with the subject How can the operation of these pumps be controlled via the Internet from the PC?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on