4/29/2024 1:46 PM | |
Joined: 4/20/2020 Last visit: 5/16/2024 Posts: 8 Rating: (0) |
Hello, I had issues compiling devices which have an OPC-UA interface. TIA just crashed every time. I did then uninstall and tried to reinstall TIA 18, but it experiences some issues with the OPCCORECOMP64 (see attachment). What could've caused it and how to fix that? For side information: I was playing around with an ASP.NET project where I used the OPCFoundation.NetStandard.Opc.Ua package and sql servers. But I think thats just local to that project and I do not suppose it would interfere with TIA. But it is a weird coincidence. AttachmentSIA_STEP7_S7FPLUS_WINCC_ADV_V18@24-04-29_14-45-08_summary.txt (12 Downloads) |
5/9/2024 4:10 AM | |
Joined: 3/30/2020 Last visit: 5/19/2024 Posts: 4514 Rating: (943)
|
Perhaps have a look at a recent conversation: Specially focus on the timestamps: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on