Industry Online Support
Technical Forum
7/24/2014 4:10 PM | |
Posts: 4 Rating: (0) |
HI all, I am also facing the problemto make MP377to communicatewith SIMATIC 505 PLC. From somewhere i got the HMIl.REC file and foundattached document. I followed the instruction mentioned in it and communication is working. But if i change the Module from middle to tiny, small or big. communication is not working. Please help me with the following queries 1.Do we need to create HMI.REC ourself or we will get with some software. As it is not with WInCC flexible installation? 2. How to make the communication work with other model size like tiny, small and big? Thanks AttachmentD:\TI505_Profibus_WinCCFlex_[1].pdf (674 Downloads) |
Last edited by: O_Moderator at: 7/30/2014 2:55 PMnew subject after splitting from /tf/WW/en/Posts/23855#top Last edited by: NavBi at: 7/24/2014 4:14 PM |
|
7/30/2014 2:56 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
Thread closed, because it is already discussed in the following thread Simatic 505 plc is not communicating with MP377 device and PC over profibus DP.. Best regards O_Moderator |
Follow us on