4/24/2024 9:44 AM | |
Joined: 1/29/2016 Last visit: 4/25/2024 Posts: 3 Rating: (0) |
Hello, I get the same kind of issue and when I check the buffer I can read : "A serious error has occurred. The system will be shut down, IFault : 20090814" "Code position: 192EAAh" "Technology package: 5F00h, start address: 40F6400h" This installation work very well since 2017 without any trouble. Yesterday I uploaded the code (very simple Boolean value!) and I downloaded the code on device. But now when I try to check the online program status with SCOUT the windows freeze few seconds, and then the Simotion D shut down !! All LEDs are blinking red very quickly 7segments display "F" If I restart the machine, the CPU power on correctly and go to RUN mode and 7 segments display "6" I have a stable online access through TIA, and SCOUT, but it's impossible to check the online program status anymore, and I need this to follow my machine troubleshooting of course !
Firmware V4.4.0 I joined the device diagnostics. ------------------------------------------------------------------------------------------ AttachmentDevice Diagnostics.txt (12 Downloads) |
Last edited by: The Helping Hand at: 04/24/2024 14:10:41New subject after splitting |
|
4/24/2024 10:04 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
this message mean that the fw on the device is crashed hve you check if a newer fw is available V4.4 HF? |
4/24/2024 3:21 PM | |
Joined: 1/29/2016 Last visit: 4/25/2024 Posts: 3 Rating: (0) |
I checked here : https://support.industry.siemens.com/cs/de/en/view/31045047 it seems I can download this fw, can you validate this is the good link/file for my device ? |
Last edited by: Jen_Moderator at: 04/25/2024 05:41:30Link optimized. |
|
4/25/2024 12:18 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
hi, this is version V5.2, if you use it you must update the FW also in the project and maybe update the Simotion Scout version(and TIA Version) depends which actual Scout/tia you use. better try first the latest V4.4 FW : |
4/25/2024 9:26 AM | |
Joined: 1/29/2016 Last visit: 4/25/2024 Posts: 3 Rating: (0) |
I updated the fw with the last 4.4 version available and now the "serious error" disappears. Thank you ! |
Follow us on