3/13/2024 7:56 PM | |
Joined: 3/13/2024 Last visit: 3/13/2024 Posts: 1 Rating: (0) |
hi dear i need more tag register more than 1000 how can increase it ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/14/2024 12:27:17New subject after splitting |
|
3/15/2024 2:55 PM | |
Joined: 7/19/2022 Last visit: 5/14/2024 Posts: 358 Rating: (61) |
Hello AutoGen_3337196, The limit of registry entries depends on the hardware device. If the limit of an HMI screen is 10,000, it is not advisable to exceed this figure. Alternatively, you can create several files to avoid overwriting older data as explained in this FAQ: How do you do long-term archiving with WinCC flexible? |
If this Information really helps, you could use the Rate function |
|
3/20/2024 11:50 AM | |
Joined: 8/3/2009 Last visit: 5/14/2024 Posts: 12944 Rating: (1647)
|
Hello what do you mean exactly with Tag registers? Do you mean Array elements? Which Device do you use? you can also check the systemlimits: https://support.industry.siemens.com/cs/ww/en/view/18796010/8994681611 Bye Murof |
If this Information really helps, you could use the Rate function |
|