4/19/2024 6:15 AM | |
Joined: 1/21/2013 Last visit: 5/15/2024 Posts: 2784 Rating: (450) |
Hi Lucas, Are you talking about swapping byte order? If so, it should be possible to do this with built-in functionality. However, it depends on the CPU you are using, and that is one of the pieces of information I am missing from your post. But in case of S7-300/400 have a look at "CAW" or in case of S7-1200/1500 have a look at "SWAP". Kind regards |
This contribution was helpful to1 thankful Users |
4/19/2024 6:24 AM | |
Joined: 11/28/2023 Last visit: 5/15/2024 Posts: 20 Rating: (0) |
Exactly what I was looking for, thank you very much
|
Follow us on