5/10/2023 9:25 AM | |
Joined: 8/3/2009 Last visit: 6/5/2024 Posts: 12991 Rating: (1659)
|
Hello thanhnhan there are systemfunctions for reading the currently logged in Username and group. ("GetUserName", "GetGroupNumber") Also for screen change there is a systemfunction available. This can also be used in a Script. If you run that script by userchange event in the Scheduler then if a user has logged in correctly you get a string or a groupnumber from the function s above. If the use logged out then you get an empty string or a 0. If you need basic help in VB SCript: https://support.industry.siemens.com/cs/ww/en/view/26150018 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on