9/17/2009 2:55 AM | |
Joined: 6/4/2008 Last visit: 6/2/2024 Posts: 1484 Rating: (322) |
Hi Sparky, out of interest, I just tried this on my project, and the Sinamics Integrated part does not show up. By the looks of it, from your piccie, you have a CBE30 card in the simotion processor option slot, this looks like a "PG/PC routing" issue. Assuming you have the OEM's original project, you can view the network setup in the Netpro editor. Please refer to the attached document, specifically theconnecting/network sections(I wrote this with a particular customer in mind, so ignore the specific IP addresses. Hope it helps P.S. Just spotted something, in your picture, the project name refers to Simotion, and your software package is Starter. Starter cannot work with Simotion devices, You need Simotion Scout which includes the full Starter functionality and more. There are many version of Scout, so I won't give a particular part number. If You have Step7 already installed, then a standard version is suitable, otherwise Scout Standalone is advised which includes the S7 hardware configurator. Discuss your requirements with your distributor. Cheers, Graeme AttachmentSimotion_Basics.pdf (765 Downloads) |
Last edited by: Graeme at: 9/17/2009 3:19 AM |
|
Follow us on