8/17/2023 8:59 AM | |
Joined: 3/7/2023 Last visit: 5/28/2024 Posts: 4 Rating: (0) |
Hi What are the two differences when I connect to port x127 or x150 when I do online in Starter? |
8/17/2023 11:25 AM | |
Joined: 5/12/2006 Last visit: 6/12/2024 Posts: 22262 Rating: (2989)
|
for connection with starter there is no difference |
This contribution was helpful to1 thankful Users |
8/22/2023 12:31 AM | |
Joined: 3/7/2023 Last visit: 5/28/2024 Posts: 4 Rating: (0) |
thanks you for your answer. then what is difference of port X127 and X150?? |
8/22/2023 8:31 AM | |
Joined: 5/12/2006 Last visit: 6/12/2024 Posts: 22262 Rating: (2989)
|
x127 -> ethernet interface for commissioning x150 -> profinet io interface for data exchange with PLC |
Follow us on