2/9/2023 10:26 PM | |
Joined: 11/4/2022 Last visit: 5/3/2024 Posts: 3 Rating: (0) |
Hi engineers! I have a seriously problem with the DCC charts. I´m in a project and I need set up with DCC. I added the DCC and I configured all I wanted but the problem occurs when I´m running the program. Example: In a logic gate (AND), I have declarated 2 entrances and I manipulated both with a 1, obviously the exit must to be 1, but in my case is a 0... I don´t know why. Can you help me? I will agregate a photo about the situation. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/10/2023 09:06:44New subject after splitting |
|
2/10/2023 9:08 AM | |
Joined: 5/12/2006 Last visit: 6/13/2024 Posts: 22262 Rating: (2989)
|
maybe the chart is not executed? have you assign it to a execution group? |
2/10/2023 2:48 PM | |
Joined: 11/4/2022 Last visit: 5/3/2024 Posts: 3 Rating: (0) |
Yeahhh I think that! And yes I did it... And the same problem still. |
Follow us on