3/9/2020 10:45 AM | |
Joined: 11/13/2019 Last visit: 7/30/2023 Posts: 2 Rating: (0) |
Hi sir, i have new cu-320-2 DP.starter is installed in my PC.PC is connected to X-127 through Ethernet.i have set PG/PC network according to the local area connection.still not able to connect through starter. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/09/2020 12:58:43New subject after splitting |
|
3/9/2020 10:51 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986) |
Hi, which FW is on the CF Card? Christoph |
4/19/2022 12:18 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986)
|
CU310-2 need a CF Card with FW to boot up! |
Follow us on