9/4/2021 12:12 AM | |
Joined: 10/13/2016 Last visit: 4/28/2024 Posts: 20 Rating: (1) |
Basically can be done, Using conversion software fro algorex to FS720, and still keep the existing devices. The only sutaible is FC723 not FC724, Since panel need Card Cage for Synoloop card, which is Analogue Plus Card and also The Interactive EX Card. Line card (SynoLOOP) FCL7201-Z3 & FCL2007-A1-Ex or you can upgrade using Line adapter (Ex) Good luck. AttachmentA6V10432669-FC723.pdf (826 Downloads) |
Follow us on