4/24/2024 9:32 AM | |
Joined: 4/24/2024 Last visit: 5/2/2024 Posts: 3 Rating: (0) |
Hello, |
Last edited by: AutoGen_5738623 at: 04/28/2024 10:25:42Last edited by: AutoGen_5738623 at: 05/02/2024 19:43:47 |
|
4/24/2024 4:32 PM | |
Joined: 6/11/2019 Last visit: 5/13/2024 Posts: 2199 Rating: (98) |
Hello AutoGen, Maybe this will help you. You still have to adapt the switching hysteresis to your circumstances. But don't choose them too small. Remember that when measuring the temperature you increase the detection range from 0-1000 to a value range of -500 to 2000 .This results in display jumps and a certain inaccuracy in the last display position. Greetings Ella_68 (translated with Google) AttachmentHeating_and_Cooling.zip (14 Downloads) |
This contribution was helpful to1 thankful Users |
4/26/2024 3:56 PM | |
Joined: 6/11/2019 Last visit: 5/13/2024 Posts: 2199 Rating: (98) |
I always use an AM2 RTD (6ED1 055-1MD00-0BA2) and the Emko temperature sensor (type: RTS-M06-L060-K02; -50 to +200°C).A PTC’s right to work is important. greeting Ella_68 |