4/6/2024 2:33 AM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32938 Rating: (4072)
|
What kind of encoder is this? What speed are we talking about? |
4/7/2024 11:17 AM | |
Joined: 1/9/2022 Last visit: 4/8/2024 Posts: 29 Rating: (0) |
encoder resolution is 100 PR |
4/7/2024 1:18 PM | |
Joined: 6/11/2019 Last visit: 5/2/2024 Posts: 2188 Rating: (98) |
- At 1155 rpm that would be 19.25 ups. - 19.25 and an incremental sensor of 1:100 that would be 1925 pulses per second. - 1925 pulses * 2 seconds sampling frequency = 3850 pulses per 2 seconds. This is possible with the logo.Therefore just set the value P4 from B002 to 100 (see example). Ella_68 AttachmentProgrammplan-3.zip (25 Downloads) |
5/2/2024 3:53 PM | |
Joined: 7/16/2021 Last visit: 5/2/2024 Posts: 1 Rating: (0) |
Can you tell me which input pin logo the PLC can use to read the high-speed pulse signal sent from the encoder? |
Follow us on