5/7/2024 6:36 AM | |
Joined: 1/21/2013 Last visit: 5/18/2024 Posts: 2795 Rating: (452)
|
Hi Kadria, Unfortunately, according to the manual, the LoggedAlarmStateResult object does not have a Name property. So you will not be able to export the alarm name. Kind regards |
5/7/2024 10:46 AM | |
Joined: 1/21/2013 Last visit: 5/18/2024 Posts: 2795 Rating: (452)
|
Hi Kadria, I looked in an existing alarm log database and saw that the name was stored there. So perhaps the name property is simply missing without being noticed during development. You can contact technical support to clarify this. A possible workaround would be to use the Database object to directly access the alarm logging database instead of the AlarmLogging object. Kind regards |
5/7/2024 11:24 AM | |
Joined: 8/5/2013 Last visit: 5/7/2024 Posts: 3 Rating: (0) |
Hi Stefan, thanks for the feedback. I contact support.. Thanks |
Follow us on