6/16/2022 11:12 AM | |
Joined: 3/16/2022 Last visit: 12/14/2022 Posts: 1 Rating: (0) |
hi all , i have TI505 PLC with me , i just wanted to read the data from PLC. i attached the pdf file about PLC please tell me which cable (Product details). i need to use, and if anywhere is available tell me the link two ports are there in this plc, Port1and Port 2 i need to connect the cable in Port 2 its DB9 cable, please Help me for this best Regards NAJI ------------------------------------------------------------------------------------------ Attachment505-8201-3.pdf (879 Downloads) |
Last edited by: CS Moderator at: 06/16/2022 20:40:01New subject after splitting |
|
6/17/2022 3:33 PM | |
Joined: 2/10/2006 Last visit: 3/21/2024 Posts: 147 Rating: (12)
|
Hi, Attached the pinout of the programming cable. it is best to build it yourself, there's no part number anymore for this cable. for further information see chapter 3.8 installing 545/555 CPU of the manual you attached. Regards, AttachmentRS232 cables.pdf (819 Downloads) |
Follow us on