|
Precision balances in integrated automationWeighing operations demanding a high degree of precision and reproducibility can now be efficiently automated. METTLER TOLEDO Standard Industrial of Greifensee, Switzerland, and Siemens Automation and Drives (A&D) of Nuremberg, Germany, offer integrated product combinations specially designed for high-precision applications in the chemicals, pharmaceuticals and food and drink industries. The Modulo WM digital weighing modules and Modulo WMH weighing platforms from METTLER TOLEDO are combined with the high resolution Siwarex FTA electronic weighing system (Flexible Technology Automatic Scale) by Siemens. Siwarex FTA is integrated into Simatic control technology or Simatic PCS-7 process control technology. The tested product combinations are certified by both companies. This new option for high-precision weighing tasks is the result of official cooperation between the two companies agreed in September 2004. The certificate for defined product combinations ensures that the components can be easily installed and that they operate without a problem.The Modulo WM weighing modules and Modulo WMH weighing platforms specially developed by METTLER TOLEDO for automated processes function based on electromagnetic power compensation and feature fast, precise weighing. The compact and sturdy housing contains both the measuring cell and all the electronics for integration into the automation solution. The product line for the WM weighing modules in a stainless steel housing is available in five different designs from a 120 g to 6 kg weighing range and resolutions between 0.1 mg and 0.01 g. The WMH weighing platforms are available in a number of versions with a weighing range from 15 kg to 3 tons and a resolution of 0.1 to 50 g. The weighing platforms with an IP67 degree of protection can be combined with a wide range of accessories. The high-resolution weighing sensors by METTLER TOLEDO are connected directly to the Siwarex FTA weighing electronics from Siemens. Having the design of a Simatic PLC module, Siwarex FTA controls weighing, filling and dosing processes precisely - even at high rates. Integrated diagnostic functions are used to monitor the weighing process, for example for quality assurance in the production process. METTLER TOLEDO is a leading worldwide manufacturer of precision instruments. The company is the world's largest manufacturer and supplier of weighing systems for laboratories, general industry and food retailers. METTLER TOLEDO is one of the three biggest suppliers of various complementary measuring technologies and is a leading supplier of systems for automated pharmaceutical research and development of active ingredients. Furthermore, the company is the world's largest manufacturer and supplier of metal detection systems in production technology and the packaging industry. For more information on METTLER TOLEDO, see their website at www.mt.com. The Siemens Automation and Drives (A&D) Group, Nuremberg, is the world's leading manufacturer in the field of automation and drives. Products supplied by A&D include standard products for the manufacturing and process industries and for the electrical installation industry as well as system solutions, for example for machine tools, and solutions for whole industries such as the automation of entire automobile factories or chemical plants. Supplementing this range of products and services, A&D also offers software for linking production and management (horizontal and vertical IT integration), as well as for optimizing production processes. A&D employs 51,800 people worldwide and in fiscal year 2004 (to September 30) earned a pre-tax profit of €1.077 billion on sales of €8.829 billion and orders of €8.98 billion. For further information: Mettler-Toledo GmbH: Marketing, Markus Gross Phone: +41 (0)44 944 25 72, E-mail: markus.gross@mt.com Information on METTLER TOLEDO at: www.mt.com Siemens: Press Office Automation and Drives, Gerhard Stauss Tel. +49 (0)911 895 7945, E-mail: gerhard.stauss@siemens.com Information on Siwarex at: www.siemens.com/siwarex This press release is available on the Internet at: www.mt.com/industrial und www.siemens.com/automation/press Download this press release (pdf): german english spanish Download this press release (doc): german english spanish You can receive this press release in electronic form. Please send us an e-mail with your request. 2005.06.23
|
||||||||||||||||||