Siemens Automation and Drives (A&D) has introduced Sitrans FUS060, a new high-performance flow meter for industrial plants.
The device is designed for applications that involve robust requirements and rely on fault-resistant measuring components, for example in the oil-refining industry, petrochemicals, power station systems or waste water purification plants. Sitrans FUS060 is ATEX-certified and disposes a Hart interface. The ultrasound device can be operated both two and four-jetly. In the four-jet mode the precision of the device improves. It enlarged the Siemens technology already being used in this area in that it enables turndown behavior of 10:1 while simultaneously meeting industrial needs for exactness and repeatability. On top of this, Sitrans FUS060 complies with OIML R117 standards and is suitable for all applications involving measurements that require calibration.
Download this press release (pdf): german english spanish Download this press release (doc): german english spanish A picture accompanies this press release. You can find this picture on the Internet at: www.siemens.com/ad-picture/1323
Reference number : A&D SC 200702.1323e |