|
Process Safety - Applications
Fire & Gas
Fire & Gas Systems are an important layer
in the overall protection scheme of industrial facilities involved in
the exploration, transportation and processing of petroleum, petrochemicals
or hazardous gases
These systems must reliably detect and alarm the presence of fire
and/or gas leaks, even under adverse conditions (ie. loss of primary system
power). Often, these same systems will automatically take action
to mitigate the consequences (i.e. suppress the fire or exhaust the gas).
Siemens as well as several of Siemens Solution Provider
partners have developed solutions based on both the QUADLOG and the SIMATIC
S7-400FH safety system platforms conforming to all relevant industry
standards. These systems are installed and performing in such arduous
environments as on oil platforms in the North Sea, on FPSOs around the
world and on wellheads on the North Slope of Alaska.
Application standards:
 |
Safety Instrumented Systems (SIS) are subject to
IEC 61511
|
 |
NFPA 72 and EN 54 describe in detail
how these systems must be constructed
|
|