Operator Panel
The operator panel has
 5 pushbuttons, of which 4 are parameterizable
 10 LEDs, of which 7 are parameterizable
The operator panel forwards all LED status dislays
for device diagnostics on the basic unit externally, thus making it possible
to control the motor feeder directly from the cabinet door, similar to a local
control point. The parameterizable pushbuttons and LEDs can be assigned to any
functions or status signals.
The system interface integrated in the front panel facilitates connection of
a PC for parameter assignment or diagnostics. Attaching an addressing plug
or memory module means Profibus addresses or even complete parameterization
of the feeder can be quickly transmitted.
The operator panel is connected at its rear system interface by means of a connection
cable to the basic unit or expansion module and is supplied by the basic unit.
The operator panel can be used for both the SIMOCODE pro C and SIMOCODE pro V device series and
with its protective system interface cover meets the requirements of the IP54 degree of protection.
User-specific pushbutton and LED labeling on the operator panel can be carried out using the SIRIUS Label Designer. |