Deutsch | Español | Français | Italiano
Site Map | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
Products
ASIsafe
Master
Slaves
Power Supply Units
Accessories
Repeaters
Extension Plugs
Adressing Units
Analyzers
Shaped Cables
M12 Branches
Flat Cable Distributors
Diagnostics
Success Stories

Adressing Units

All devices in the AS-Interface network must be addressed in order to be able to exchange data with the master. This means that the devices must be assigned an address value. This can be realized offline using the addressing unit or online using the AS-Interface master. Addresses have values of between 1 and 31 or 1A to 31A and for the extended address mode, 1B to 31B. A new slave has the address 0. Using the addressing unit, it is also possible to read and write slave data offline – such as the slave profile, ID codes, parameters (e.g. for analog slaves).
Print
   

© Siemens AG 2001-2008 - Corporate Information - Privacy Policy - Terms of Use