Power Supply Units
AS-Interface power supplies are an integral component of the AS-Interface network.
They generate a regulated 30V DC with a high degree of stability and low residual
ripple. They are used to supply the electronics of the AS-i network
– i.e. AS-i modules and the master as well as the connected sensors. Through
the integrated data coupling, the power supplies reliably isolate data and power
that are simultaneously transferred along the AS-i cable.
|