Deutsch | Español | Français | Italiano
Site Map | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
[Advanced]
Products
Success Stories
Airport
Sorting Plant
Automotive Industry
Insulating Material
Special-Purpose Machine Building
Crane System
CD Production
Distributed Motor Starter Solutions
BMW Wackersdorf
VW Wolfsburg
AS-i/PROFIBUS

Conveying Systems at VW Wolfsburg in Germany

Smooth Wheel Rim Transports Thanks to AS-Interface

Everything runs smoothly with AS Interface: the new conveyor section for rims at VW Wolfsburg, Germany.
The starters are directly next to the drives: 46 AS Interface compact starters help cut costs.
Distributed motor starter concept reduces required control cabinet volume by 60%!
An everyday occurrence at VW Wolfsburg: hour after hour, hundreds of wheel rims on their way to the welding unit travel along the new 400 meter long conveyor section made by Wegener+Stapel of Bergen, Germany. To enable easy adjustment to varying rim demand, the new conveyor system needed to be of flexible design. And as far as flexibility is concerned, AS Interface meets these requirements perfectly.
Consistent distribution – reasons and advantages:
14 AS Interface masters in the conveyor section ensure that the VW rims get to where they're needed just in time for further assembly.
46 AS Interface compact starters look after the drive.
As a result of the distributed design, the motor starters are fed by a local power bus, thus minimizing the length of the motor line to the switching device.
The distributed design reduces the required control cabinet volume by 60%.
The motors can be started and tested in manual mode, independent of PLC.
Saves time on documentation: hardly any cable connection plans required.
"AS Interface not only makes commissioning easier but more economic, too. We were able to put the conveyor section into operation bit by bit and integrate it in the manufacturing process without once interrupting rim production."
(Jürgen Lange from Wegener+Stapel)
Print
   

© Siemens AG 2001-2009 - Corporate Information - Privacy Policy - Terms of Use