Deutsch
Sitemap | Contact Us | Index
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support
Login | Register
link to related website
Picture S7-200

Demo software: STEP 7-Micro/WIN test version 4.0 E

With STEP 7-Micro/WIN software you'll enjoy the full benefit of all the advantages of SIMATIC S7-200. Exceptionally powerful tools make your daily work easier and save you time and money. The intuitive wizards simplify the configuration of communications, and the new Supertree provides an optimized project overview as well as fast access to all segments of the user program. The interactive control panels for positioning as well as PID Autotuning support the commissioning process even more efficiently than in the past.

The various wizards of STEP 7-Micro/WIN enable you to use convenient parametering in the place of programming. All the steps in the process are made a lot simpler: All you need to do is enter a few parameters – aided by menus – to generate an executable program at the touch of a few keys.

Download and installation instructions:

1. To download the related files click the filename, then click "save". The files can be saved in a directory of your choice. Repeat the process and save the files in the same directory.

2. As soon as all files are saved in the directory, click the "rejoin.bat" file. This causes the test version to be consolidated into a single .exe file.

3. To proceed with the installation, double-click the .exe file. This saves all Installs files in a temporary subdirectory on your PC and starts the installation.

4. Follow the instructions of the installation program.

5. When the installation is complete, the temporary subdirectory with the installation routines can be deleted. This action must be performed manually.


Please note:

•The single license of STEP 7-Micro/WIN V4.0 cannot be installed on a PC on which a V4.0 test version is installed. The V4.0 test version must be uninstalled before the single license is installed.

• The test version supports the following languages: German, English, Spanish, French, Italian, Chinese.

• Your purchase of STEP 7-Micro/WIN V4.0 includes tools: TD Keypad Designer for TD 200C, and S7-200 Explorer for the S7-200 Memory Cartridge. The test version does not include these tools. However, they can be downloaded separately from the Siemens A&D Service and Support Web site.

• This test version provides the full functionality of the normal product for 60 days. It can be started up to 100 times.

After a presumably successful test you can purchase the single license with the order number 6ES7810-2CC03-0YX0.

Order number for any updates: 6ES7810-2CC03-0YX3.


System requirements for the test version:

  • At least 265 Mb free space disk
  • Microsoft Windows 2000 (SP3 or higher) or Windows XP (Home or Professional)
  • A PC that meets these requirements
  • Monitor resolution 1024x768 pixels with small font size
  • A mouse supported by Microsoft Windows
  • Additional hardware from one of the following:
    • 1 PC/PPI cable connected to the RS-232 interface (PC COM1 or COM2)
    • 1 PC/PPI cable connected to the USB interface
    • 1 communications processor card (CP) and Multipoint interface cable (MPI)
    • 1 Multipoint interface card (MPI) (the communications cable is included)
    • 1 PC Ethernet connection with the S7-200 CP243-1 or CP243-1 IT module

Print
   

© Siemens AG 2006-2010 - Corporate Information - Privacy Policy - Terms of Use