|
| Productivity-Boosting Systems |
| The Siemens booth, with its two futuristic cylinders, will showcase numerous interesting innovations.
|
|
|
| Flexible and Highly Productive |
| Sinumerik 840D powerline performs demanding control and drive functions in innovative milling-turning centers.
|
|
|
| Kinematics "Virtually" Secured |
| Mechatronic Support from Siemens validates new kinematics concept for innovative automatic production lathes.
|
|
|
| Simulation for Greater Productivity |
| Mechatronic Support from Siemens aids in the achievement of ambitious turbine blade production goals.
|
|
|
| Ultra-Dynamic Hardening |
| Eldec Schwenk Induction GmbH in Dornstetten, Germany, uses Sinumerik, Simodrive and Vision sensors in its induction-hardening systems in order to ensure that the best possible procedure is in place for applying significantly increased generator power to components.
|
|
|
| Performance plus Flexibility |
| A machining center must not be merely fast, precise and dependable. It must also be possible to integrate it seamlessly into the existing production environment. Scherer Feinbau has implemented these demands in vertical turning centers which have already proven themselves in the harsh everyday life of production. Thirty of these state-of-the-art machines will be going on line at Audi in Ingolstadt in the near future.
|
|
|
| Fast Retooling |
| As part of a pilot project, the MAKA Max Mayer Maschinenbau company developed a new machining center for wooden, aluminum and plastic door machining. With its minimal space requirements and flexible applications options, it also offers vocational businesses the opportunity of implementing automatic machining. Equipped with state-of-the-art control and drive technology, the machining center for doors meets all of the company's expectations in terms of speed and flexibility.
|
|
|
| A Vision Based on Experience |
| Reichenbacher Hamuel has been manufacturing CNC machining centers for over 30 years. However, the earliest machines and those of the newest generation really only have the basic concept in common. The two latest products on display at LIGNA 2007 were consistently improved with the help of innovative control and drive generation.
|
|
|
| New Dimension |
| The new Pro-Master CNC machining center from HolzHer-Reich Spezialmaschinen enables perfect 5-axis machining of all types of wooden parts. In addition to its vibration-free operation, the modern Sinumerik 840D solution line control system also plays a key role in the machine's performance, providing optimal results even for high-speed cutting.
|
|
|
| Perfect precision |
| As a high technology trendsetter, the Weinig company has significantly expanded the possibilities for complete processing of workpieces with its Profiling Center Conturex. To ensure perfect precision, the world's leading manufacturer of machines for solid wood processing has once again chosen to rely on digital control and drive technology from Siemens.
|
|
|
| With Teamwork to New Solutions |
| For years, Deckel Maho Seebach GmbH has been utilizing direct drives in its vertical machining centers which enhance the productivity of the end-user. During this process, the cooperation with Mechatronic Support results in shorter development times and a perfect harmony between mechanical system, drive and control.
|
|
|
| More Efficiency for Smooth Finish |
| Supfinas new Planet V series grinding machines illustrates that great increases in quality are possible during face grinding by utilizing standard automation and drive technology. It is also possible to increase the productivity of the machine by around 500 percent by using the Sinumerik 840D.
|
|
|
| Performance plus Flexibility |
| Currently, a machining center must not be merely fast, precise and dependable. It must also be possible to integrate it seamlessly into the existing production environment. Scherer Feinbau has implemented these demands in vertical turning centers which have already proven themselves in the harsh everyday life of production. Thirty of these state-of-the-art machines will be going on line at Audi in Ingolstadt in the near future.
|
|
|
| Sharp scrutiny |
| In the cylinder head production section at DaimlerChrysler, Germany's largest automobile manufacturer, robust and reliable vision sensors from Siemens are used to identify the fitted parts using a data matrix code. The technology ensures parts traceability, an indispensable aspect of today's quality management processes.
|
|
|
| More Functions |
| CNC Design recently decided to endeavour into another technology by retrofitting a Leifeld PNC350-19/2 Spinning Machine at Murdock Metal Spinning in Melbourne, Australia. This model of Leifeld's Spinning Machines was designed to be self programming, hence, having the ability of learning from the operator and accurately playing it back.
|
|
|
| Machine update with many advantages |
| Volvo brought a transfer line for the processing of brake discs in their component factory in Floby in Sweden up to the latest state of the automation art. The Siemens service team managed to complete the retrofit of the complex system in less than ten weeks.
|
|
|
| Ultra-fast from "Down Under" |
| H&H Machine Tools has developed a 5-axes high-speed mill for a renowned Malaysian aerospace supplier. The Australian partner of Siemens CNC Design provided the automation of the ultra-fast "Ultra 5" with Sinumerik 840D, Simodrive 611D and linear motors 1FN3.
|
|
|
| Twice as Productive |
| To further reduce the machining times for series workpieces, Honsberg introduced the Mach 1-500 Synchro at EMO 2005, which is equipped with two spindles operating fully in synch. The machine builder cooperated with Siemens as the system vendor on the project, which provided all of the electrical equipment, including the switchgear cabinet construction.
|
|
|
| Dynamic and Flexible |
| Trumpf has had 3D laser machining cells in its product line for several years. With the new TruLaser Cell Series 7000, the concept was once again significantly improved, especially regarding its usability, productivity and modularity. The new machine is controlled with Sinumerik and Simodrive technology.
|
|
|
| Test Run - As Close As It Gets |
| Previously, anyone who wanted to simulate production processes on the computer could not do without complex simulation programs which could only be operated by specially trained employees. A new Siemens Solution Partner is now offering a solution which even small companies can afford, and which combines simple operation with intelligent 3D technology.
|
|