|
|
| | Graphic programming of drive-related functions for Simotion and Sinamics | At this year's Hannover trade fair, Siemens Automation and Drives (A&D) will be demonstrating its Drive Control Chart (DCC) for complete graphic programming of technological functions for the Simotion Motion Control system and the Sinamics S120 drives series. With DCC, function blocks with multi-instance capability from a standard library are linked to each other and parameterized graphically. The technical closed-loop control structures are clearly displayed in the process. The user is thus provided with new ways of easily adapting Simotion and Sinamics to the specific functions of a machine.
With the DCC editor from Siemens A&D, open-loop and closed-loop control functions can be configured very easily. Function blocks with multi-instance capability are selected from a predefined library and graphically linked to each other with the drag-and-drop function. DCC is not subject to any restrictions regarding the number of usable functions. The open-loop and closed-loop control structure created by means of DCC is displayed clearly. Existing diagrams can easily be displayed and reused. Testing and diagnostic functions make it possible to verify the program response or to identify causes in the event of a fault.
The function block library encompasses a large selection of control, mathematical and logic blocks as well as extensive open-loop and closed-loop control functions. For logical linking, evaluation and acquisition of binary signals, all the standard logic functions are available such as AND, XOR, on/off delays, RS memory or counter. For monitoring and evaluation of numerical variables, there are many mathematical functions available, such as absolute value generation, dividers, and minimum/maximum evaluation. In addition to the closed-loop control of drives, coilers, PI controllers, ramp generators or wobble generators can be configured without difficulty.
For the Sinamics S120 drive series, Drive Control Chart also provides an easy-to-use basis for solving drive-related tasks in the converter, thus taking the load off a higher-level control unit. The machine processes can be configured much more easily. Local processing in the drive leads to an improvement in the overall machine performance. In conjunction with the Simotion Motion Control system, almost unlimited programming of technical control structures is possible. They can then be combined with other program parts to form one overall program.
You can find more information on the Internet at: www.siemens.de/sinamics-s120 and www.siemens.de/simotion
Download this press release (pdf): german english spanish Download this press release (doc): german english spanish A picture accompanies this press release. You can find this picture on the Internet at: www.siemens.com/ad-picture/1418
Reference number: AD MC 200702.1418e |  |
|
|
|