|
Nuremberg, 2009-09-30
Product Lifecycle Management for Machine ToolsAt this year's EMO trade show for machine tools to be held from October 5 through 10 in Milan, Siemens will be exhibiting a range of comprehensive software solutions for complex product lifecycle management (PLM) tasks across the entire process chain. The portfolio extends from computer-aided product development at the CAD/CAM level up to virtual machines, and considerably shortens time-to-market for machine builders while also enhancing product quality and productivity for end user customers.
The software portfolio of the Siemens presentation at this year's EMO focuses on the workpiece-oriented process chain between the initial idea for the product and the finished part. The software fully covers the requirements for sophisticated product lifecycle management tasks in the machine tool industry. This begins with product development using CAD/CAM systems and the generation of programs for parts, via optimization of the post processor and the CNC parameters and extends to offline simulations for validating and optimizing the manufacturing process..
NX software from Siemens provides an open and versatile 3D system at the CAD/CAM/CAE level for the entire design and manufacturing process. NX facilitates the construction of full 3D models using the latest technology for fast and easy model creation and editing. Specifications defined during the design phase such as manufacturing tolerances and finish are attached to the 3D CAD models as Product and Manufacturing Information (PMI). The full 3D geometric model and the attached data such as PMI is available later in the process for manufacturing engineering and can be used directly in NX CAM to drive NC programming selections.
NX CAM includes NX Post Builder an application which makes it easy to create a post-processor exactly suited to a customer’s machine tool and specifically prepared for SINUMERIK controllers.
The tightly connected NX post processor automatically adjusts the part program based on machine operations such as roughing, semi-finishing and finishing and related machining data inside NX CAM. To that end Siemens PLM Software has introduced a range of new functions in NX CAM including a set of menu options available to the NC programmer to allow these special options that drive key elements of the advanced functions on Siemens’ Sinumerik controller to be selected during NC programming. Another important element of the workpiece-oriented process chain is the “Virtual Machine” software package for machine tools with Sinumerik CNC controllers. This includes a version of the software from the real controller, (known as the virtual Numeric Control Kernel - VNCK), the machining simulation system (RealNC) for 3D model based simulation with gouge and collision detection, as well as the original Sinumerik HMI software for operating the virtual controller and machine. The Virtual Machine simulation facilitates extremely realistic simulation on a standard PC of the NC machining processes. This level of simulation can be used to effectively eliminate programming errors and possible collisions. Job changeover times are considerably shortened as a result of thorough validation and set-up checking on the virtual machine. By more efficient programming, shorter changeover times and reducing the error risk, simulation of the production processes with the "Virtual Machine" software system helps to optimize manufacturing processes and thus raise productivity.
You can find further information on the Internet at:
www.siemens.de/sinumerik
Download this press release (pdf):
Download this press release (doc): A picture accompanies this press release. You can find this picture on the Internet at: www.siemens.com/ad-picture/2014 Reference number: IDT2009.09 2014e fp Contact partner: volker.banholzer@siemens.com
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||