|
Nuremberg, 2009-10-20
Process control system Simatic PCS 7 LAB for micro process engineeringEhrfeld Mikrotechnik BTS GmbH (EMB), a Bayer Technology Services GmbH company, and the Siemens Industry Automation Division jointly adapted the process control system Simatic PCS 7 LAB for use in micro process engineering, particularly for controlling the EMB modular micro reaction system.
The combination of modules of EMB’s micro reaction system creates a reaction plant performing chemical synthesis to develop solutions for the chemical, pharmaceutical and life science industries. Specially tailored to laboratory requirements, the Simatic PCS 7 LAB monitors the processes of these plants; it controls, records and logs the relevant process variables such as pressure, temperature and flow rate. Thanks to an easy-to-use library, the engineering of the process control system becomes child’s play. Technical information as well as parameter settings of the modules are stored as symbols in a library. To create an image of the plant, these symbols can be arranged and combined on a panel according to the plant configuration. Predefined functions and interfaces to external devices are already integrated.
"As a result of this collaboration, our customers benefit from the global-player expertise of Siemens: worldwide service and support, along with on-site user training", commented Dr. Olaf Stange, managing director of Ehrfeld Mikrotechnik BTS GmbH.
Further information can be found on the Internet at: www.siemens.de/simatic-pcs7-lab
Download this press release (pdf):
Download this press release (doc): A picture accompanies this press release. You can find this picture on the Internet at: www.siemens.com/ad-picture/2106 Reference number: IIA200907.2106e fp Contact partner: julia.kauppert@siemens.com
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||