Deutsch
Sitemap | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support  |  About Us
Login | Register
[Advanced]
Publications
Press Center
Press Releases
Press Newsletter
Speeches/ Presentations
Press Contact
Press Archive
Picture Archive
Management
Analyst Relations
Events & Trade Shows
Newsletter

Nuremberg, 2009-03-06

New operator panel for standard drives

Siemens Drive Technologies is exhibiting its new Sinamics IOP (Intelligent Operator Panel) at this year´s Hannover Fair. This new panel has simplified operation and plain text displays to speed up commissioning and shorten downtimes. That raises machine and plant availability and consequently productivity. This IOP has been designed for the Sinamics G120, G120D and G110D standard drives, and the Simatic ET200 frequency converter. New operator panel for standard drives
The outstanding feature of the Siemens Sinamics IOP (Intelligent Operator Panel) is its user-friendliness. This benefits both the operator with little prior knowledge and the experienced drive expert. The large plain text display, menu-based operation with rotary knob, and the integrated application wizards make commissioning standard drives much easier. Plain text parameter displays, help texts and a parameter filter usually enable a drive to be commissioned without a printed parameter list. Application wizards guide the user interactively through the commissioning of applications, such as pumps, fans, compressors and materials-handling drives. Process variables can be monitored directly on the IOP status display, so that faults are detected and rectified quickly. The Sinamics IOP helps not only to speed up commissioning but also to drastically reduce the length of planned and unplanned downtimes, so increasing machine and plant availability.
 
This operator panel has been designed for the Sinamics G120, G120D and G110D standard drive series, and the Simatic ET200 frequency converter. Depending on the type of converter, the IOP can either be mounted on the drive or in the control cabinet door, or alternatively used as a mobile handheld unit. The IOP has an integrated USB interface to make expansions and reading in new software versions easy.
 
You can find further information on the Internet at: www.siemens.com/sinamics-g120
 
Download this press release (pdf):
german english spanish

Download this press release (doc):
german english spanish

A picture accompanies this press release. You can find this picture on the Internet at: www.siemens.com/ad-picture/2001

Reference number: IDT2009.03 2001e fp

Contact partner: volker.banholzer@siemens.com

Print
   

© Siemens AG 2001-2009 - Corporate Information - Privacy Policy - Terms of Use