Deutsch
Sitemap | Contact Us
Home  |  Products & Solutions  |  News Center  |  e-commerce  |  Support  |  About Us
Login | Register
[Advanced]
Publications
Press Center
Press Releases
Press Newsletter
Speeches/ Presentations
Press Contact
Press Archive
Picture Archive
Management
Analyst Relations
Events & Trade Shows
Newsletter

Nuremberg, 2009-09-23

Innovative user interface for machine tools

With Sinumerik Operate, Siemens Drive Technologies has integrated the control and programming interfaces HMI-Advanced, ShopMill and ShopTurn in a single end-to-end interface for machine tools. Sinumerik Operate contains animated elements and allows intuitive operation and programming. New functions mean that even complex workpieces are easy to set up and manufacture in a clamp. Innovative user interface for machine tools
At this year's EMO trade fair, Siemens Drive Technologies will be exhibiting the new end-to-end user interface Sinumerik Operate on the new computerized numerical control Sinumerik 828D and Sinumerik 840D sl for the first time. Sinumerik Operate integrates the established user and programming interfaces HMI-Advanced, ShopMill and ShopTurn in a single interface for machine tools. It enables sequence and high-level language programming in a single interface and thereby ensures fast NC programming and work preparation. The clearly-structured layout with context-based functions and self-explanatory icons facilitates intuitive handling for machine operators. Various different kinematics are also easy to set up, while integrated simulations and a large number of diverse workpiece views also make it easy to check the programming immediately. It is also possible to zoom into angled levels individually while a simulation is running.
 
When setting up a workpiece, the measurements are shown in an easy-to-understand
way using animated elements, both for switched and manual tool measurement features. With the Cycle 800 “swivel cycle” it is possible to manufacture even extremely complex workpieces in a clamp with simple and fast handling. With the new Sinumerik Operate user interface, users now have access to an optimized tool and program management system. The tool list makes all relevant data available in a clearly structured manner and also offers a configurable display. Thanks to its use of context-based functions and self-explanatory icons, it is also simple and intuitive to use.
 
With the innovative Sinumerik Operate user interface, the familiar, tried and tested programming methods are available. The ShopMill and ShopTurn sequence programming constitutes a tailor-made programming solution for the manufacture of individual parts and small batch sizes. The programGUIDE brings together G-Code programming with cycle support. This ensures a high degree of flexibility and short machining times, and is above all suitable for medium to large batch sizes.

You can find further information on the Internet at: www.siemens.de/sinumerik
 
Download this press release (pdf):
german english spanish

Download this press release (doc):
german english spanish

A picture accompanies this press release. You can find this picture on the Internet at: www.siemens.com/ad-picture/2018

Reference number: IDT2009.09 2018e fp

Contact partner: volker.banholzer@siemens.com

Print
   

© Siemens AG 2001-2009 - Corporate Information - Privacy Policy - Terms of Use