|
Nuremberg, 2009-03-10
IT maintenance and service solutions for enhanced machine availabilityAt this year’s Hannover Messe, Siemens is presenting maintenance and service concepts for increasing the availability of machines and plant. Condition-based maintenance and fault detection are the basis of the solutions, such as Sinumerik Manufacturing Excellence, that are on display at the fair. They enable plant operators to achieve substantial cuts in the operating costs and expenditures connected with downtimes, repairs and spare part ware-housing.
Lifecycle costs, productivity and machine availability: They are the keywords used to describe the demands that plant operators place on automation systems in order to lower the cost of production. Another requirement calls for the reduction of unit costs, they themselves being heavily influenced by the current expenditure for the operation of a plant. Holistic concepts and services for machines promise tremendous potential for the optimization of costs and expenditures over the lifecycle of a machine or plant. Increasingly important in this respect is preventive maintenance and, therefore, the plannability of downtimes. This year in Hannover, the two Siemens’ Drive Technologies and
IT Solutions and Services Divisions will show new solutions for condition-based maintenance and fault detection in production, fault registration and ticketing in maintenance, and mobile devices that can be used by service technicians fault rectification. The IT-based service concepts and processes from Siemens use intelligent sensors and programs for continuous diagnosis of the condition of a machine or plant, thereby enabling the necessary spare part supplies and related downtimes to be scheduled in good time. The scope of these solu-tions offered by Siemens ranges from the facility of remote access over the entire fault and main-tenance management systems to the products and systems required for condition monitoring. Em-ploying automatic processes, they make it possible to monitor the condition of a machine or plant on a continuing basis. Trend analyses and comparisons with the so-called stored plant fingerprint permit the early detection of critical developments in machine components, thus giving the plant operator more time to plan or even immediately adopt appropriate measures. Integrated reporting functions support the focused elimination of the causes of faults. Owing to its modular design, Sinumerik Manufacturing Excellence from Siemens can be readily adapted to the specific demands of any plant or application.
You can find further information on the Internet at: www.siemens.de/sinumerik/manufacturing-excellence
Download this press release (pdf):
Download this press release (doc): Reference number: IDT2009.03 2004e fp Contact partner: volker.banholzer@siemens.com
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||