2008-08-28
With the standardized and open interfaces of the Sinumerik 840D sl control, Siemens enables simple integration of robots into the shop floor area. Users of machine tools can use this to convert flexibly to automatic or series production in addition to standard tasks.
more
|
2008-08-22
Siemens has expanded its portfolio of industrial software with an agreement to acquire innotec GmbH of Schwelm, Germany, an international vendor of digital engineering software and services for the process industry.
more
|
2008-08-08
The Siemens Industry Automation Division has added new components to its Simatic PCS 7 Lab process control system, specially tailored to suit laboratory requirements. This process control system is based on the compact Box PC.
more
|
2008-06-24
The new Sitrans LVL100 and LVL200 vibratory switches from the Siemens Industry Automation Division are suitable for signaling when the level of liquid media is sufficiently high, liquid media is required or needs to be refilled, and for protecting pumps.
more
|
2008-06-18
The Siemens Industry Automation Division has developed an all-inclusive kit for verifying the accuracy and performance of flowmeters of any brand or type.
more
|
2008-06-06
The Siemens Industry Automation Division has equipped the mainboards of its rugged industrial PC family with a Profinet interface. Designed as a three-port switch, this supports isochronous real time and integrates the Siemens PC into Profinet networks.
more
|
2008-06-03
Siemens will present its portfolio, which is designed for the needs of European electronics manufacturers, at this year’s SMT Hybrid Packaging Trade Show in Nuremberg.
more
|
2008-05-30
The new Sitrans FX300 vortex flowmeter series of the Siemens Industry Automation Division is equipped with a pressure sensor and a temperature sensor. By combining these in one unit, the vortex principle is used to measure the temperature, pressure and flow of steam, gases and liquids.
more
|
2008-05-30
A free library for applications in the water and wastewater industry now exists for the Simatic PCS 7 process control system. The Simatic Water Library of the Siemens Industry Automation Division supplements the PCS 7 engineering system with over 100 proven and re-usable modules for automation and operator control.
more
|
2008-05-28
Integrated drive packages for the graphics industry and modular automation solutions for printing machines are the focal points of the presentation made by Siemens Drive Technologies at the Drupa 2008 trade fair in Düsseldorf.
more
|
previous
|
next
|